XDPP1148-100B_version 11-0x5437E6BF.txt is the configuration file that can be loaded through the GUI.
Usually we don't need to load XDPP1148-100B_version 11-0x5437E6BF.txt.
Just connect the board with GUI and then follow the below steps to start up:
1.Connect the GUI with the board.
2.Power the input voltage to the input voltage range.(375Vdc-410Vdc)
3.Set the register "tlm_vin_force" value to 700(Decimal) in the Register Map column
4.Set the Command "OPERATION" to "Output ON" in the PMB column.
Then the board will soft-start up.